Trelleborg’s Latest Perfluoroelastomer Material Meets Demanding Enhanced Oil Recovery Requirements

HOUSTON, TX and FORT WAYNE, IN (May 1, 2017) –Trelleborg Sealing Solutions uses the Offshore Technology Conference in Houston as a platform to launch its latest Isolast® perfluoroelastomer material development.

Perfluoroelastomer Material

Specifically engineered for the offshore industry, Isolast® J9554 matches up to the most demanding of upstream requirements and is ideally suited for Enhanced Oil Recovery (EOR) systems.

Chris Busby, Product Manager for Isolast® material, says: “To achieve extended sealing life in demanding environments, it is important that sealing materials specified match up to the conditions likely to be faced. A particular focus for development of Isolast® J9554 was ensuring long seal life in EOR systems. This includes thermal recovery where heat is introduced to the oil reservoir to reduce the viscosity of the oil and cyclic steam injection, which is used extensively in heavy-oil reservoirs and tar sands to thin oil and enhance its ability to flow.”

Extensive testing was undertaken to prove that Isolast® J9554 can operate at the extreme temperatures and pressures encountered in critical upstream applications, including high temperature steam environments. The material exhibited excellent retention of physical properties following high temperature steam aging for one week at +300°C / +572°F.

Isolast® J9554 delivers exceptional chemical resistance and high thermal stability in harsh oil and gas environments. A high hardness, high modulus material with excellent long-term retention of physical properties, it is ideally suited to high pressure applications where high thermal stability and resistance to aggressive well bore chemicals such as amine-based corrosion inhibitors, steam and acids, are vital to ensure reliable seal performance.

The material demonstrates excellent compression set retention at high temperatures with temperature resistance from +14 °F/ -10 °C to +527 °F/ +275 °C with excursions to +572 °F/ +300 °C. In addition to EOR applications, the material is also suited to use in downhole tools and chemical dosing pumps.

Comments are closed.